SPRACY3 June 2021 F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1 , TMS320F280023C , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040C-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280048C-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28076 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
At the beginning, GPIO8 and GPIO9 are configured as EPWM5A and EPWM5B, while GPIO10 and GPIO11 are configured as EPWM6A and EPWM6B, respectively. Secondly, use Input X-BAR to select the related GPIO pins for EPWM5B and EPWM6B.
XBAR_setInputPin(XBAR_INPUT3,9); // INPUT X-BAR 3 = GPIO9 = EPWM5B
XBAR_setInputPin(XBAR_INPUT4,11); // INPUT X-BAR 4 = GPIO11 = EPWM6B
Then, use CLB X-BAR to select the INPUT X-BAR INPUT 3 and INPUT4 as AUXSIG1 and AUXSIG2. In this example, CLB Tile 1 can be also used to handle the delayed protection for EPWM5B and EPWM6B, together with EPWM1B.
//for EPWM5B/EPWM6B input to CLB
XBAR_setCLBMuxConfig(XBAR_AUXSIG1, XBAR_CLB_MUX05_INPUTXBAR3);
XBAR_enableCLBMux(XBAR_AUXSIG1, XBAR_MUX05);
XBAR_setCLBMuxConfig(XBAR_AUXSIG2, XBAR_CLB_MUX07_INPUTXBAR4);
XBAR_enableCLBMux(XBAR_AUXSIG2, XBAR_MUX07);
CLB_configLocalInputMux(CLB1_BASE, CLB_IN3, CLB_LOCAL_IN_MUX_GLOBAL_IN);
CLB_configLocalInputMux(CLB1_BASE, CLB_IN4, CLB_LOCAL_IN_MUX_GLOBAL_IN);
CLB_configGlobalInputMux(CLB1_BASE, CLB_IN3, CLB_GLOBAL_IN_MUX_CLB_AUXSIG1);
CLB_configGlobalInputMux(CLB1_BASE, CLB_IN4, CLB_GLOBAL_IN_MUX_CLB_AUXSIG2);
CLB_configGPInputMux(CLB1_BASE, CLB_IN3, CLB_GP_IN_MUX_EXTERNAL);
CLB_configGPInputMux(CLB1_BASE, CLB_IN4, CLB_GP_IN_MUX_EXTERNAL);