SPRAC71A March 2019 – February 2020
Copy tables is the term for a general capability in the TI Toolchain to facilitate moving data from offline storage to online storage. Offline storage generally refers to where the program is loaded; it could be ROM, slower memory, and so on. Online storage generally refers to where the data resides when the program runs. The data being copied can be either code or variables. The term copy table refers to a table of source and destination addresses in which objects to be copied are registered. There is also a runtime component in the form of library functions that read the table and perform the copying in response to calls in the program.
There are numerous applications for copy tables, but the two most common are:
The copy table mechanism is not part of the ABI. The means by which initialized variables get their initial values is by contract between the linker and the run-time library, which are required to be from the same toolchain. However, there may be advantages for other toolchains to follow the TI mechanism, or there may be a need for downstream tools to recognize the format, so we document it here.
The following figure illustrations the general mechanism. An object file contains an initialized section, .mydata in the example. At link time, the user specifies that .mydata is to have separate load and run addresses, and specifies that a copy table entry be created for it. The linker removes the data from .mysect, making it an uninitialized section, and assigns its address as its run location. It creates a new initialized section called .mydata.load1 which contains .mydata‟s data in encoded form, and places it at the load location. It links in a function called copy_in from the run-time library to decode and copy the data at run time, as well as additional format-specific helper functions. Finally, it creates a section (.ovly1 in the example) that contains a copy table, which is a sequence of copy records that point to the source data and the destination address, and a handler table (not shown) that the copy function uses to choose the right decode helper function.
At run time, the application invokes copy_in to decompress and copy the data. The argument to copy_in is the address of the copy table associated with the section. The function parses the table and executes the specified copy operations.
Multiple objects can be encoded and registered for copy-in. Each generates its own copy table in the .ovly (1)section.
Figure 14-1 Copy
Table OverviewA few variations are possible: