SPRAC71A March 2019 – February 2020
C28x object files use a section naming convention that provides improved granularity while retaining the convenience of default rules for combining sections at link time. A section whose name contains a colon is called a subsection. Subsections behave as normal sections in all respects, but their name guides the linker when combining sections into output files. The root name of a subsection is the name up to, but not including, the colon. The suffix includes all characters following the colon. By default, the linker combines all sections with matching roots into a single section with that name. For example, .text, text:func1, and .text:func2 are combined into a single section called .text. The user may be able to override this default behavior in toolchain-specific ways.
If there are multiple colons, section combination proceeds recursively from the right-most colon. For example. unless the user specifies otherwise, the default rules combine .bss:func1:var1 and .bss:func1:var2, which then combine into .bss.
Subsections whose root names match special sections have the same ABI-defined properties as the section they match, as defined in Section 11.4.5. For example .text:func1 is an instance of a .text section.