SPRAC71A March 2019 – February 2020
Some fields of the EXIDX and EXTAB tables need to record program memory addresses or pointers to other locations in the tables, both of which are typically in code or read-only segments. To facilitate position independence, this is done using a special-purpose PC-relative relocation called R_C28x_PREL31, abbreviated here as PREL31. A PREL31 field is encoded as a scaled, signed 31-bit offset which occupies the least significant 31 bits of a 32-bit word. The remaining (most significant) bit is used for different purposes in different contexts. The relocated address to which the field refers is found by left-shifting the encoded offset by 1 bit and adding it to the address of the field.