SPRAC71A March 2019 – February 2020
The GC++ABI defines a class's key function, whose definition triggers creation of the virtual table for that class, to be the first non-pure virtual function that is not inline at the point of class definition. The C28x ABI modifies this to be the first non-pure virtual function that is not inline at the end of the translation unit. In other words, an inline member is not a key function if it is first declared inline after the class definition.