SPRAC71A March 2019 – February 2020
A compact EXTAB entry is indicated by a 1 in bit 31 of the first word. (When an EXTAB entry is encoded into the second word of an EXIDX entry, the compact form is always used.) In the compact form, the personality routine is encoded by a 4-bit PR index in the first byte of the entry. The remaining 3 bytes contain unwinding instructions as specified by the personality routine. In a non-inlined EXTAB entry, additional data is provided in additional successive 32-bit words: any additional unwinding instructions, followed optionally by action descriptors, terminated with a NULL word.