SPRAC71A March 2019 – February 2020
A weak function is a function whose symbol has binding STB_WEAK. A program can successfully link without a definition of a weak function, leaving references to it unresolved.
The ABI supports calls to imported weak functions; that is, functions potentially defined in a different static link unit. If a reference to a weak function remains unresolved at link time, the linker replaces its address with zeros. The user is responsible for adding a check that the address is not zero or NULL before attempting to call a weak function.