SPRAC71A March 2019 – February 2020
Prior to release 18.12.0.LTS of TI's C28x Compiler Tools , the one and only ABI for C28x was the original COFF-based ABI. It was strictly a bare-metal ABI; there was no execution-level component.
Release 18.12.0.LTS of the TI Compiler Tools introduced a new ABI called the C28x EABI. It is based on the ELF object file format. It is derived from industry standard models, including the IA-64 C++ ABI and the System V ABI for ELF and Dynamic Linking. The processor-specific aspects of the ABI, such as data layout and calling conventions, are largely unchanged from the COFF ABI, although there are some differences. Needless to say, the COFF ABI and the EABI are incompatible; that is to say, all of the code in a given system must follow the same ABI. TI's compiler tools support both the new EABI and the older COFF ABI, although we encourage migration to the new ABI as support for the COFF ABI may be discontinued in the future.
A platform is the software environment upon which a program runs. The ABI has platform-specific aspects, particularly in the area of conventions related to the execution environment, such as the number and use of program segments, addressing conventions, visibility conventions, pre-emption, program loading, and initialization. Currently bare metal is the only supported platform. The term bare metal represents the absence of any specific environment. That is not to say there cannot be an OS; it simply says that there are no OS-specific ABI specifications. In other words, how the program is loaded and run, and how it interacts with other parts of the system, is not covered by the bare-metal ABI.
The bare-metal ABI allows substantial variability in many specific aspects. For example, an implementation may provide position independence (PIC), but if a given system does not require position independence, these conventions do not apply. Because of this variability, programs may still be ABI-conforming but incompatible; for example if one program uses PIC but the other does not, they cannot interoperate. Toolchains should endeavor to enforce such incompatibilities.