SLAZ742A July 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0G3507-Q1
Peripheral registers are still accessible after disabling PWREN register
B
When disabling the power of a peripheral by setting the PWREN register to 0, the peripherals registers may appear to retain data values if read. Reading or writing to the registers when PWREN is 0 has no affect as the peripheral has no effect.
The following peripherals are affected: comparator (COMP), operational amplifier (OPA), TimerA, TimerG, general-purpose input/output (GPIO), and windowed watchdog timer (WWDT), AES and TRNG.
When the PWREN register of the peripheral is set to 0, the values of the associated registers should be disregarded or considered invalid.