SDAA172 March 2026 AM13E23019
On AM13E230x devices, UART is configured by the device ROM code to the following default configurations:
| UART Signal | Device Signal Name | Pin Name | GPIO # | Mux Mode |
|---|---|---|---|---|
| UART RX | UC4_RX_SCL_SCLK | PA1 | GPIO1 | 7 |
| UART TX | UC4_TX_SDA_PICO | PA0 | GPIO0 | 7 |
Having these signals available on a header can aid in debugging a prototype system and make sure that the device is booting properly at power-on. For these reasons, it is highly recommended that this UART interface is accessible on the PCB system.