SDAA114A September 2025 – July 2026 AMC0211D , AMC0211D-Q1 , AMC0211R , AMC0211R-Q1 , AMC0211S , AMC0211S-Q1 , AMC0230D , AMC0230D-Q1 , AMC0230R , AMC0230R-Q1 , AMC0230S , AMC0230S-Q1 , AMC0311D , AMC0311D-Q1 , AMC0311R , AMC0311R-Q1 , AMC0311S , AMC0311S-Q1 , AMC0330D , AMC0330D-Q1 , AMC0330R , AMC0330R-Q1 , AMC0330S , AMC0330S-Q1 , AMC0336 , AMC0380D , AMC0380D-Q1 , AMC0380R , AMC0380R-Q1 , AMC0381D , AMC0381D-Q1 , AMC0381R , AMC0381R-Q1 , AMC1211-Q1 , AMC1311 , AMC1311-Q1 , AMC1350 , AMC1350-Q1 , AMC1351 , AMC1351-Q1 , AMC1411 , AMC1411-Q1 , AMC3311 , AMC3311-Q1 , AMC3330 , AMC3330-Q1
Figure 3-1 shows the experimental board used for obtaining the test data. The experimental board has three isolated amplifiers with different output type (single-ended fixed gain, single-ended ratiometric output and differential output). Additionally, the board contains a modulator device that is not a subject of this application note.
Figure 3-2 and Figure 3-3 show the performance of two different operational amplifiers in the identical setup using the TMS320F28P650 microcontroller with 16-bit 1-MSPS multiplexed ADC. The sample and hold time is tSMPL=425ns.
Figure 3-1 Experimental Test SetupWaveforms in Figure 3-2 represent the OPA365. A high-performance, high-bandwidth (50MHz), rail-to-rail operational amplifier. This is visible during the three scenarios described previously, the operational amplifier output settles in less than 150ns. Waveforms in Figure 3-3 represent TLV9001, a low-cost, 1MHz bandwidth rail-to-rail operational amplifier. This is visible that the operational amplifier output requires more than 800ns to settle for the same three test conditions. As a consequence, the sample and hold switch opens before the input of the ADC has settled. This is visible especially for the undershoot scenario when VSH<VOUT. In this case the voltage used for AD conversion is 30mV higher than this needs to be. This is resulting in 1% reading error for a 3V voltage reference used in the system.