SBAU171D May 2010 – January 2016 ADS1198 , ADS1298
The input of the ADS1x98ECG-FE requires a DB15 connector. Figure 45 illustrates the most optimal cable connection to the ADS1298ECG-FE. Figure 46 and Figure 47 show two alternate ways that cables can be constructed to interface with the ADS1x98ECG-FE. Figure 48 shows an alternate testing tool to the instrument used in the tests for this user guide (refer to Section 5.7.1).
Figure 45. 15-Pin, Shielded Connector from Biometric Cables
Figure 46. 15-Pin, Twisted Wire Cable to Banana Jacks
Figure 47. 15-Pin, Twisted Wire Cable
Figure 48. Cardiosim ECG Simulator Tool