ZHCSS31 september   2020 TSB41BA3F-EP

PRODUCTION DATA  

  1.   1
  2. 1 特性
  3. 2 应用
  4. 3 说明
  5. 4 Revision History
  6. 5 Terminal Configuration and Functions
    1.     Terminal Functions
  7. 6 Specifications
    1. 6.1 Absolute Maximum Ratings
    2. 6.2 ESD Ratings
    3. 6.3 Recommended Operating Conditions
    4. 6.4 Thermal Information
    5. 6.5 Electrical Characteristics - Driver
    6. 6.6 Electrical Characteristics - Receiver
    7. 6.7 Electrical Characteristics - Device
    8. 6.8 Switching Characteristics
  8. 7 Operating Life Deration
  9. 8 Parameter Measurement Information
  10. 9 Overview
  11. 10Functional Block Diagram
  12. 11Principles Of Operation (1394b Interface)
    1. 11.1 LLC Service Request
    2. 11.2 Status Transfer
    3. 11.3 Receive
    4. 11.4 Transmit
  13. 12Principles Of Operation (1394a-2000 Interface)
    1. 12.1 LLC Service Request
    2. 12.2 Status Transfer
    3. 12.3 Receive
    4. 12.4 Transmit
    5. 12.5 Interface Reset and Disable
  14. 13Applications, Implementation, and Layout
    1. 13.1 Known exceptions to functional specification (errata).
      1. 13.1.1 Errata # 1:Restore from Leaf Node (Nephew)
        1. 13.1.1.1 Detailed Description
        2. 13.1.1.2 Background
        3. 13.1.1.3 Workaround Proposal
        4. 13.1.1.4 Corrective Action
    2. 13.2 Application Information
      1. 13.2.1 Interoperability with earlier revisions of TSB41BA3
      2. 13.2.2 Internal Register Configuration
      3. 13.2.3 Feature Enhancements to revision F
        1. 13.2.3.1 Detect Loss of Descrambler Synchronization
          1. 13.2.3.1.1 Detect Loss of Descrambler Synchronization Advantages and Uses
        2. 13.2.3.2 Fast Retrain
          1. 13.2.3.2.1 Fast-Retrain Advantages and Uses
          2. 13.2.3.2.2 Fast-Retrain Backward Compatibility
        3. 13.2.3.3 Fast Power-On Re-connect
          1. 13.2.3.3.1 Fast Power-On Re-Connect Advantages and Uses
          2. 13.2.3.3.2 Fast Power-On Re-Connect Backward Compatibility
        4. 13.2.3.4 Fast Connection Tone Debounce
        5. 13.2.3.5 Programmable invalidCount
      4. 13.2.4 Power-Class Programming
      5. 13.2.5 Using The TSB41BA3F-EP With A 1394-1995 Or 1394a-2000 Link Layer
      6. 13.2.6 Power-Up Reset
      7. 13.2.7 Crystal Selection
      8. 13.2.8 Bus Reset
      9. 13.2.9 Designing With Powerpad™ Devices
  15. 14Device and Documentation Support
    1. 14.1 Tools and Software
    2. 14.2 Device Nomenclature
    3. 14.3 Documentation Support
    4. 14.4 支持资源
    5. 14.5 Trademarks
    6. 14.6 静电放电警告
    7. 14.7 术语表
  16. 15Mechanical, Packaging, and Orderable Information
    1. 15.1 Packaging Information
    2. 15.2 Mechanical Data

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

Crystal Selection

The TSB41BA3F-EP and other Texas Instruments PHY devices are designed to use an external 49.152-MHz crystal connected between the XI and XO terminals to provide the reference for an internal oscillator circuit. This oscillator in turn drives a PLL circuit that generates the various clocks required for transmission and resynchronization of data at the S100 through S400 media data rates.

A variation of less than ±100 ppm from nominal for the media data rates is required by IEEE Std 1394. Adjacent PHYs can therefore have a difference of up to 200 ppm from each other in their internal clocks, and PHYs must be able to compensate for this difference over the maximum packet length. Larger clock variations can cause resynchronization overflows or underflows, resulting in corrupted packet data or even PHY lockup.

For the TSB41BA3F-EP, the PCLK output can be used to measure the frequency accuracy and stability of the internal oscillator and PLL from which it is derived. When operating the PHY-LLC interface with a non-1394b LLC, the frequency of the PCLK output must be within ±100 ppm of the nominal frequency of 49.152 MHz. When operating the PHY-LLC interface with a 1394b LLC, the frequency of the PCLK output must be within ±100 ppm of the nominal frequency of 98.304 MHz.

The following are some typical specifications for crystals used with the physical layers from Texas Instruments in order to achieve the required frequency accuracy and stability:

  • Crystal mode of operation: Fundamental
  • Frequency tolerance at 25°C: Total frequency variation for the complete circuit is ±100 ppm. A crystal with ±30 ppm frequency tolerance is recommended for adequate margin.
  • Frequency stability (over temperature and age): A crystal with ±30 ppm frequency stability is recommended for adequate margin.
Note:

The total frequency variation must be kept below ±100 ppm from nominal with some allowance for error introduced by board and device variations. Trade-offs between frequency tolerance and stability can be made as long as the total frequency variation is less than ±100 ppm. For example, the frequency tolerance of the crystal can be specified at 50 ppm, and the temperature tolerance can be specified at 30 ppm to give a total of 80 ppm possible variation due to the oscillator alone. Aging also contributes to the frequency variation.

  • Load capacitance: For parallel resonant mode crystal circuits, the frequency of oscillation depends on the load capacitance specified for the crystal. Total load capacitance (CL) is a function of not only the discrete load capacitors, but also board layout and circuit. It might be necessary to select discrete load capacitors iteratively until the PCLK output is within specification. It is recommended that load capacitors with a maximum of ±5% tolerance be used.

As an example, for the OHCI + 41LV03 evaluation module (EVM), which uses a crystal specified for 12-pF loading, load capacitors (C9 and C10 in Figure 13-8) of 16 pF each were appropriate for the layout of that particular board. The load specified for the crystal includes the load capacitors (C9, C10), the loading of the PHY terminals (CPHY), and the loading of the board itself (CBD). The value of CPHY is typically about 1 pF and CBD is typically 0.8 pF per centimeter of board etch; a typical board can have 3 pF to 6 pF or more. The load capacitors C9 and C10 combine as capacitors in series so that the total load capacitance is:

GUID-8FF3624F-13FA-41E9-82A3-E064C7C8527A-low.gif
GUID-3BC144EE-BC92-4664-B5D0-A5B020B9E9F9-low.gifFigure 13-8 Load Capacitance for the TSB41BA3F-EP PHY
Note:

The layout of the crystal portion of the PHY circuit is important for obtaining the correct frequency, minimizing noise introduced into the PHY's phase-locked loop, and minimizing any emissions from the circuit. The crystal and two load capacitors must be considered as a unit during layout. The crystal and load capacitors must be placed as close as possible to one another while minimizing the loop area created by the combination of the three components. Varying the size of the capacitors can help in this. Minimizing the loop area minimizes the effect of the resonant current (IS) that flows in this resonant circuit. This layout unit (crystal and load capacitors) must then be placed as close as possible to the PHY XI and XO terminals to minimize trace lengths.

GUID-585150D7-CB62-4976-AD80-0FC142801809-low.gifFigure 13-9 Recommended Crystal And Capacitor Layout

It is strongly recommended that part of the verification process for the design be to measure the frequency of the PCLK output of the PHY. This should be done using a frequency counter with an accuracy of six digits or better. If the PCLK frequency is more than the crystal's tolerance from 49.152 MHz or 98.304 MHz, then the load capacitance of the crystal can be varied to improve frequency accuracy. If the frequency is too high, add more load capacitance; if the frequency is too low, decrease the load capacitance. Typically, changes must be done to both load capacitors (C9 and C10 in Figure 13-9) at the same time, and both must be of the same value. Additional design details and requirements can be provided by the crystal vendor.