ZHCSUF1 January 2024 TPS7H3014-SP
ADVANCE INFORMATION
The TPS7H3014 is a four-Channel, 3V to 14V, sequencer and supervisor for space applications. The device is intended to drive devices with enable high logic inputs. The channel count can be incremented as needed for the application by connecting multiple ICs. in a daisy-chain configuration. Each output incorporates a push-pull architecture. The logic high of these outputs are externally provided by the user by supplying a voltage to the PULL-UPx inputs. All ENx push-pull outputs are tied to the PULL_UP1 domain while SEQ_DONE and PWRGD are tied to the PULL_UP2 domain.
The SENSEx inputs are connected to the non-inverting input (undervoltage) of a comparator which is used to determine the on (in regulation) and off (not in regulation) voltage level of the monitored power supply (VOUTx). Each of these inputs feature a threshold level of 599mV (typ) with an accuracy of ±1% across: voltage, temperature, and radiation (TID). The hysteresis voltage threshold level can be adjusted by the user and determined by the RTOPx resistance and the hysteresis current (IHYS). The IHYS becomes active once the rising voltage at SENSEx exceeds the threshold (599mV typ), indicating the monitored voltage rail is in regulation. IHYS is 24μA with an accuracy of ±3% across: voltage, temperature, and radiation (TID).
The device incorporates two timers:
Separate UP and DOWN pins are provided by the device in order to enable daisy-chain configurations. The UP pin has a threshold (VTH _UP) of 599mV (typ), while the DOWN pin has an threshold (VTH _DOWN) of 498mV. A fixed hysteresis of 100mV is incorporated in both input comparators for noise stability. These pins are edge sensitive, a rising edge in UP starts the sequence up, while a falling edge in DOWN will start the sequence down.
When using a single device and driven externally, both pins (UP and DOWN) are typically tied together. Since UP and DOWN inputs have an accurate threshold, they can be used to initiate the sequence up and down by accurately sensing another rail (using a resistive divider), or they can be externally driven by a controller. Once UP is driven above VTH _UP, the device will start a sequence up by asserting EN1 high after the programmed delay time (DLY_TMR), at which point the SENSE1 will start rising up. If SENSE1 crosses the on voltage before the REG_TMR is expired, then EN2 will be asserted high after the programmed delay. This process continues until the SEQ_DONE and PWRGD are asserted high indicating a complete sequence up and system power good, respectively.
Once the DOWN pin is driven below VTH_DOWN, the device will start a sequence down by forcing EN4 low after the programmed delay. At this point, the SENSE4 voltage will start falling until is lower than the set off voltage. Once this happens, EN3 will be asserted low after the programmed delay. This will continue until EN1 is forced low. As the discharge time of the sequenced devices is unknown, the REG_TMR is not active during power down.
During sequence up, SEQ_DONE and PWRGD are asserted high after the last used channel crosses the on voltage threshold and the programmed DLY_TMR is expired (assuming it is active). During sequence down, SEQ_DONE is forced low once VOUT1 is below the off voltage and the DLY_TMR is expired. However PWRGD is forced low immediately after the commanded sequence down.
The TPS7H3014 also incorporates a comprehensive FAULT management system described in the State Machine section.