ZHCS614G October 2011 – September 2022 TPS40422
PRODUCTION DATA
Figure 6-1 RHA Package40-Pin VQFNTop View
Figure 6-2 RSB Package40-Pin WQFNTop View| PIN | NO. | I/O | DESCRIPTION |
|---|---|---|---|
| ADDR0 | 10 | I | Low-order address pin for PMBus address configuration. One of eight resistor values must be connected from this pin to AGND to select the low-order octal digit in the PMBus address. |
| ADDR1 | 9 | I | High-order address pin for PMBus address configuration. One of eight resistor values must be connected from this pin to AGND to select the high-order octal digit in the PMBus address. |
| AGND | 6 | — | Low-noise ground connection to the controller. Connections should be arranged so that power level currents do not flow through the AGND path. |
| BOOT1 | 30 | I | Bootstrapped supply for the high-side FET driver for channel 1 (CH1). Connect a capacitor (100 nF typical) from BOOT1 to SW1 pin. |
| BOOT2 | 20 | I | Bootstrapped supply for the high-side FET driver for channel 2 (CH2). Connect a capacitor (100 nF typical) from BOOT2 to SW2 pin. |
| BP3 | 32 | O | Output bypass for the internal 3.3-V regulator. Connect a 100 nF or larger capacitor from this pin to AGND. The maximum suggested capacitor value is 10 µF. |
| BP6 | 25 | O | Output bypass for the internal 6.5-V regulator. Connect a low ESR, 1 µF or larger ceramic capacitor from this pin to PGND. The maximum suggested capacitor value is 10 µF. |
| BPEXT | 24 | I | External voltage input for BP6 switchover function. If the BPEXT function is not used, connect this pin to PGND via a 10-kΩ resistor. Otherwise connect a 100-nF or larger capacitor from this pin to PGND. The maximum suggested capacitor value is 10 µF. |
| CLK | 12 | I | Clock input for the PMBus interface. Pull up to 3.3 V with a resistor. |
| CNTL1 | 4 | I | Logic level input which controls startup and shutdown of CH1, determined by PMBus options. When floating, the pin is pulled up to BP6 by an internal 6-µA current source. |
| CNTL2 | 5 | I | Logic level input which controls startup and shutdown of CH2, determined by PMBus options. When floating, the pin is pulled up to BP6 by an internal 6-µA current source. |
| COMP1 | 3 | O | Output of the error amplifier for CH1 and connection node for loop feedback components. |
| COMP2 | 7 | O | Output of the error amplifier for CH2 and connection node for loop feedback components. For two-phase operation, use COMP1 for loop feedback and connect COMP1 to COMP2. |
| CS1N | 35 | I | Negative terminal of current sense amplifier for CH1. |
| CS2N | 17 | I | Negative terminal of current sense amplifier for CH2. |
| CS1P | 34 | I | Positive terminal of current sense amplifier for CH1. |
| CS2P | 18 | I | Positive terminal of current sense amplifier for CH2. |
| DATA | 11 | I/O | Data input/output for the PMBus interface. Pull up to 3.3 V with a resistor. |
| DIFFO1 | 39 | O | Output of the differential remote sense amplifier for CH1. |
| FB1 | 2 | I | Inverting input of the error amplifier for CH1. Connect a voltage divider to FB1 between DIFFO1 and AGND to program the output voltage for CH1. |
| FB2 | 8 | I | Inverting input of the error amplifier for CH2. Connect a voltage divider to FB2 between VOUT2 and GND to program the output for CH2. For two-phase operation, use FB1 to program the output voltage and connect FB2 to BP6 before applying voltage to VDD. |
| GSNS1 | 38 | I | Negative terminal of the differential remote sense amplifier for CH1. |
| GSNS2 | 14 | I | Negative terminal of the differential remote sense amplifier for CH2. |
| HDRV1 | 29 | O | Bootstrapped gate drive output for the high-side N-channel MOSFET for CH1. |
| HDRV2 | 21 | O | Bootstrapped gate drive output for the high-side N-channel MOSFET for CH2. |
| LDRV1 | 27 | O | Gate drive output for the low side synchronous rectifier N-channel MOSFET for CH1. |
| LDRV2 | 23 | O | Gate drive output for the low-side synchronous rectifier N-channel MOSFET for CH2. |
| PGND | 26 | — | Power GND. |
| PG1 | 33 | O | Open drain power good indicator for CH1 output voltage. |
| PG2 | 19 | O | Open drain power good indicator for CH2 output voltage. |
| RT | 1 | I | Frequency programming pin. Connect a resistor from this pin to AGND to set the oscillator frequency. |
| SMBALRT | 13 | O | Alert output for the PMBus interface. Pull up to 3.3 V with a resistor. |
| SW1 | 28 | I | Return of the high-side gate driver for CH1. Connect to the switched node for CH1. |
| SW2 | 22 | I | Return of the high-side gate driver for CH2. Connect to the switched node for CH2. |
| SYNC | 40 | I | Logic level input for external clock synchronization. When an external clock is applied to this pin, the controller oscillator is synchronized to the external clock and the switching frequency is one half of the external clock frequency. When an external clock is not used, tie this pin to AGND. |
| TSNS1 | 36 | I | External temperature sense input for CH1. |
| TSNS2 | 16 | I | External temperature sense input for CH2. |
| VDD | 31 | I | Power input to the controller. Connect a low ESR, 100 nF or larger ceramic capacitor from this pin to AGND. |
| VSNS1 | 37 | I | Positive terminal of the differential remote sense amplifier for CH1. |
| VSNS2 | 15 | I | Positive terminal of the differential remote sense amplifier for CH2. |