ZHCSQT2 March 2024 ADS127L18
ADVANCE INFORMATION
The gain calibration value is a 24-bit word consisting of three 8-bit registers coded in straight-binary format and normalized to unity gain at 400000h. For example, to correct a gain error greater than 1, the compensating gain value is less than 400000h. Table 7-12 shows example gain calibration values. The ordering of the three-byte gain value is the low address for the most-significant byte. See the CHn_Gain register for the gain register addresses of each channel.
GAIN REGISTER VALUE | GAIN APPLIED |
---|---|
433333h | 1.05 |
400000h | 1 |
3CCCCCh | 0.95 |