SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
For SDRAM data integrity, the MSMC2DDR bridge supports inline ECC on the data written to or read from the SDRAM. ECC is enabled by programming the bits in the DDR16SS_ECC_CTRL_REG register. ECC is stored together with the data so that a dedicated SDRAM device for ECC is not required.
8-bit single error correction double error detection (SECDED) ECC is calculated over 64-bit data quanta. For every 512-byte data block 64 bytes of ECC is stored inline. Thus 1/9th of the total SDRAM space is used for ECC storage and the rest 8/9th is available for system use. From system point of view that 8/9th of the SDRAM data space are seen as consecutive byte addresses. Even if there are non-ECC protected regions the previously described 1/9th-8/9th rule still applies and consecutive byte addresses are seen from system point of view. Note that 8/9 of the total SDRAM space is available for system use regardless of the size of the ECC region(s). In other words, only 8/9 of the memory is available even in non-ECC regions when ECC is enabled.
The ECC is calculated for all accesses that are within the address ranges protected by ECC. The address ranges are specified through the following registers:
Note that the addresses in these address range registers should be in terms of the DDRSS address space, not the SoC memory space. Even though the SoC memory space for DDR may be split into multiple regions, the DDRSS address space is continuous.
For example, if the beginning of DDR is in SoC memory space 0x8000_0000 to 0xFFFF_FFFF, this corresponds to DDRSS address space 0x00000000 to 0x7FFFFFFF. If the SoC has greater DDR address reach, even at a discontinuous address, the address range for these registers would be continuous (eg, if the next DDR address at the SoC level is 0x880000000, the corresponding address would be continuous at 0x80000000)
Note that the value programmed in the ECC range start/end registers does not include the lower 16 bits of the address. For example, to represent an address of 0x40000000, the register contents would be 0x4000.
The ECC is read and verified during reads if both the DDR16SS_ECC_CTRL_REG[0] ECC_EN and DDR16SS_ECC_CTRL_REG[2] ECC_CK bits are set to 0x1. For 1-bit ECC error, the MSMC2DDR bridge corrects the data and returns it to the requestor. Although the error is corrected on the returned data, the SDRAM is not corrected. It is responsibility of the system software to correct the ECC error at that location.
It is also responsibility of the system software to pre-load the ECC protected region with known data before functional reads and writes are performed. This can be done by writing to the SDRAM with ECC enabled (DDR16SS_ECC_CTRL_REG[0] ECC_EN = 0x1 and DDR16SS_ECC_CTRL_REG[1] RMW_EN = 0x1) and ECC check disabled (DDR16SS_ECC_CTRL_REG[2] ECC_CK = 0x0). Once the data is loaded in the SDRAM, ECC check must be enabled (DDR16SS_ECC_CTRL_REG[2] ECC_CK = 0x1) before using the DDR interface.