SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
If there is a timeout on PCIe or an abort, PCIE_PHY_LOCAL_LEVEL interrupt will be issued. The PCIE_PHY_LOCAL_LEVEL interrupt is generated by the aggregation of the LOCAL_INTERRUPT and PHY_INTERRUPT_OUT signals from the PCIe core. For more details, see the PCIe specification.