ZHCSDT4D June 2015 – September 2020 BQ29209-Q1
PRODUCTION DATA
请参考 PDF 数据表获取器件具体的封装图。
Higher cell balancing currents can be supported by means of a simple external network, as shown in Figure 9-3.
The VC1_CB pin is tri-stated when cell balancing is disabled, is driven low by the internal logic to enable balancing on CELL1, and is driven high by the internal logic to enable balancing on CELL2. RCLAMP ensures that both Q1 and Q2 remain off when balancing is disabled, and should be sized above 2 kΩ to prevent excessive internal device current when the balancing network is activated. If RCLAMP is too small, then the gate-source voltage required to enable the external FETs cannot be achieved. RCBext determines the value of the balancing current, and is dependent on the voltage of the balanced cell and the specific Q1 and Q2 transistors used in the design (due to the transistors operating in saturation mode during balancing). The balancing currents (assuming the current through RCLAMP is not significant) are given as follows: