TIDUEW7 May   2020

 

  1.    Description
  2.    Resources
  3.    Features
  4.    Applications
  5.    Design Images
  6. 1System Description
    1. 1.1 Key System Specifications
  7. 2System Overview
    1. 2.1 Block Diagram
    2. 2.2 Design Considerations
      1. 2.2.1 Processor – i.MX 6ULL Applications Processor
      2. 2.2.2 i.MX 6ULL Memory Interfaces
        1. 2.2.2.1 DDR3L
        2. 2.2.2.2 Quad SPI NOR Flash
        3. 2.2.2.3 eMMC iNAND
        4. 2.2.2.4 SD Card Connector
      3. 2.2.3 USB to UART Converter
      4. 2.2.4 USB Ports
      5. 2.2.5 LCD Screen Connector
      6. 2.2.6 JTAG Header
      7. 2.2.7 USB2ANY Header
      8. 2.2.8 Functional Switches and Status LEDs
      9. 2.2.9 GPIO Expansion Connector
    3. 2.3 Highlighted Products
      1. 2.3.1 TPS6521815 - Power Management IC
      2. 2.3.2 DP83849I - Dual Ethernet PHY
      3. 2.3.3 INA3221 - Current Monitor
      4. 2.3.4 Reset Scheme
      5. 2.3.5 TPS2054B, TPS22964C - Auxiliary Load Switches
    4. 2.4 System Design Theory
      1. 2.4.1 Power Estimation
      2. 2.4.2 Power Sequencing
      3. 2.4.3 I2C Device Chain
      4. 2.4.4 Clock Scheme
      5. 2.4.5 BOOT Configuration
      6. 2.4.6 PCB Floor Planning
  8. 3Getting Started, Testing Setup, and Test Results
    1. 3.1 Getting Started with Hardware and Software
      1. 3.1.1 Hardware
        1. 3.1.1.1 On-board LED Information
      2. 3.1.2 Software
        1. 3.1.2.1 Booting of TIDA-050043
        2. 3.1.2.2 Example Linux Commands for Testing TIDA-050043
  9. 4Design Files
    1. 4.1 Schematics
    2. 4.2 Bill of Materials
    3. 4.3 CAD Files
    4. 4.4 Gerber Files
    5. 4.5 Assembly Drawings
  10. 5Software Files
  11. 6Related Documentation
    1. 6.1 Trademarks
    2. 6.2 Third-Party Products Disclaimer

Hardware

This section contains information about the initial set-up of the TIDA-050043 board, power-up options and user interfaces. Figure 23 shows the top side of the fully assembled PCB with labels to help locate connectors or switches on the boards.

Figure 23. Top of TIDA-050043 PCB With LabelsTIDA-050043 050043_218-MX6Y_Photo1a-Top-lbls.gif

Figure 24 shows the bottom side of the fully assembled PCB with labels.

Figure 24. Bottom of TIDA-050043 PCB With LabelsTIDA-050043 050043_218-MX6Y_Photo2a-Bot-lbls.gif

The following is a list of steps that must be followed to set up the hardware of the system.

  1. Attach stand-offs to the board with screws inserted in the four holes at the edge of the PCB.
  2. Set the BOOT option using SW7/SW6 DIP switches (Figure 25 and Figure 26).
  3. Insert CR2032 coin-cell battery in the holder BH1 (Figure 27).
  4. Insert the SD card in J2 connector, if SD Card is used for BOOT (Figure 28).
  5. Insert the USB micro-B cable into J8 connector for UART debug in Terminal window (Figure 29). Type-A plug connects to computer USB port
  6. Insert the 5-V DC adapter barrel jack into J1 connector to supply power (Figure 30). SMI24-5-V-P6 from CUI Inc is the recommended power supply.
  7. Set SW1 to the ON position.
  8. After BOOT is complete, connect the desired peripherals. For example: RJ-45 Ethernet (J3), LCD screen (J9), USB device (J4, J5, J6, J7).
Figure 25. Setting DIP Switch (SW7) for BOOT Mode from Internal MemoryTIDA-050043 050043_218-MX6Y_Photo5-Boot1-SW7.gif
Figure 26. Setting DIP Switch (SW6) for BOOT Config from SD CardTIDA-050043 050043_218-MX6Y_Photo6-Boot2-SW6.gif
Figure 27. Inserting Coin Cell Battery Into BH1TIDA-050043 050043_218-MX6Y_Photo8-CoinCell-BH1.gif

NOTE

The voltage of the coin-cell battery (3.0 V nominal) must be above 2.4 V for the supervisor to allow system power-on. If the coin-cell battery voltage is too low, it must be replaced with a fresh battery to continue testing.

Figure 28. Inserting SD Card Into J2TIDA-050043 050043_218-MX6Y_Photo7-SD.gif
Figure 29. Inserting micro-B Cable Into J8TIDA-050043 050043_218-MX6Y_Photo10-InsertUART.gif

NOTE

Refer to Section 3.1.2 for the procedure to debug TIDA-050043 through Terminal window

Figure 30. Inserting 5-V DC Adapter Into J1TIDA-050043 050043_218-MX6Y_Photo11-InsertPWR.gif

NOTE

Power supplies other than the SMI24-5-V-P6 may be substituted if the DC output voltage, current rating, polarity, and barrel jack size (inside diameter and outside diameter) are equivalent. Power supplies with DC voltage greater than 5.25V are not acceptable because of the over voltage protection circuit on the board which is intended to prevent damage to the ICs.

NOTE

It is always recommended to power-down the system by switching SW1 to the OFF position before unplugging the DC adapter power supply.