SWRA715 December 2021 CC2642R , CC2652R
The hid_emu_kbd project is a Bluetooth Low Energy project that implements the HOGP specification on the CC26x2 devices. The project uses the Bluetooth peripheral role as specified by the HOGP specification. The project demos the mouse, keyboard, and consumer report portions of the HOGP. Through the use of notifications and the GATT profile, the project is able to implement HID over Bluetooth Low Energy and properly interface with an HID Host. The hid_emu_kbd project has several complex parts that are discussed in this document. These parts come together in order to implement the overall functionality.