SWRA715 December 2021 CC2642R , CC2652R
The consumer report notifications have a payload that is comprised of a single byte. The byte corresponds to the Consumer Control ID that is being sent. An example of a consumer report notification payload that is generated by this project is “0A” which would be parsed by the HID Host as shown in Figure 4-8.
Figure 4-8 Parsed Consumer Report
Notification Payload