SWRA715 December 2021 CC2642R , CC2652R
The hardware/software used during the development of this project and the hardware/software expected to be used is displayed in Table 5-1.
| PC Operating System | Windows 10 – 64 Bit |
| Development Board | LAUNCHXL-CC26X2R1 |
| SDK Version | SimpleLink CC13x2 26x2 SDK 5.10 |
| IDE Version | CCS 10.3 |
The HOGP implementation should function with any properly implemented HID Host, but it was only extensively tested in the environment mentioned above. The latest released version of the HOGP BLE project can be found in the Texas Instruments GitHub. This example will be updated periodically as needed.