SWRA603A March 2018 – May 2019 CC1100 , CC1101 , CC110L , CC1120 , CC1121 , CC1125 , CC113L , CC1150 , CC115L , CC1175 , CC1190 , CC1200 , CC1201 , CC1310 , CC1312PSIP , CC1312R , CC1314R10 , CC1350 , CC1352R , CC1402P , CC1404P , CC1407P , CC2530 , CC2531 , CC2538 , CC2540 , CC2541 , CC2590 , CC2591 , CC2592 , CC2640 , CC2642R , CC2642R-Q1 , CC2650 , CC2650MODA , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP
In a RF system having the best possible range is important in many cases. There are many factors that can cause poor range. This application report provides a step-by-step guide on which parts of the design could cause shorter range than desired.
| Term | Definition |
|---|---|
| Conducted | The DUT is connected via cable directly to the instrument. |
| Radiated | Over the air |
| CW | Carrier Wave (tone) |