SWRA603A March   2018  – May 2019 CC1100 , CC1101 , CC110L , CC1120 , CC1121 , CC1125 , CC113L , CC1150 , CC115L , CC1175 , CC1190 , CC1200 , CC1201 , CC1310 , CC1312PSIP , CC1312R , CC1314R10 , CC1350 , CC1352R , CC1402P , CC1404P , CC1407P , CC2530 , CC2531 , CC2538 , CC2540 , CC2541 , CC2590 , CC2591 , CC2592 , CC2640 , CC2642R , CC2642R-Q1 , CC2650 , CC2650MODA , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP

 

  1.   Debugging Communication Range
  2.   Trademarks
  3. 1Calculate the Theoretical Range
  4. 2Determine Root Cause
  5. 3Measure the Conducted Sensitivity
  6. 4Measure the Conducted Output Power
  7. 5Antenna Measurements
  8. 6Still Issues?
  9. 7References
  10. 8Revision History

Measure the Conducted Output Power

  1. Disconnect the antenna and perform conducted measurements at the SMA connector or solder on a semi-rigid coax cable at the 50 Ω point.
  2. Preferred: Use a Spectrum analyzer. MSP-SA430 or similar does not have the required accuracy. Use 1 MHz RBW for measuring output power and unmodulated carrier on the transmitter.
  3. If a SA is not available, then use an EM or Launchpad with a SMA connection point.
    1. Add a known RF attenuation block between the transmitter’s SMA connector (50 Ω point) and the EM/Launchpad connector.
    2. Use SmartRF Studio and set the EM/Launchpad in continuous RX and read the RSSI.
  4. If the conducted power is poor:
    1. Is the schematic according to the reference design?
    2. Is the layout according to the reference design?