SPNA232A July 2016 – October 2019 RM41L232 , RM41L232 , RM42L432 , RM42L432 , RM44L520 , RM44L520 , RM44L920 , RM44L920 , RM46L430 , RM46L430 , RM46L440 , RM46L440 , RM46L450 , RM46L450 , RM46L830 , RM46L830 , RM46L840 , RM46L840 , RM46L850 , RM46L850 , RM46L852 , RM46L852 , RM48L530 , RM48L530 , RM48L540 , RM48L540 , RM48L730 , RM48L730 , RM48L740 , RM48L740 , RM48L940 , RM48L940 , RM48L950 , RM48L950 , RM48L952 , RM48L952 , RM57L843 , RM57L843 , TMS5700405-Q1 , TMS5700405-Q1 , TMS570LC4357 , TMS570LC4357 , TMS570LC4357-EP , TMS570LC4357-EP , TMS570LS0232 , TMS570LS0232 , TMS570LS0332 , TMS570LS0332 , TMS570LS0432 , TMS570LS0432 , TMS570LS0714 , TMS570LS0714 , TMS570LS0714-S , TMS570LS0714-S , TMS570LS0914 , TMS570LS0914 , TMS570LS10106 , TMS570LS10106 , TMS570LS10116 , TMS570LS10116 , TMS570LS10206 , TMS570LS10206 , TMS570LS1114 , TMS570LS1114 , TMS570LS1115 , TMS570LS1115 , TMS570LS1224 , TMS570LS1224 , TMS570LS1225 , TMS570LS1225 , TMS570LS1227 , TMS570LS1227 , TMS570LS20206 , TMS570LS20206 , TMS570LS20206-EP , TMS570LS20206-EP , TMS570LS20216 , TMS570LS20216 , TMS570LS20216-EP , TMS570LS20216-EP , TMS570LS2124 , TMS570LS2124 , TMS570LS2125 , TMS570LS2125 , TMS570LS2134 , TMS570LS2134 , TMS570LS2135 , TMS570LS2135 , TMS570LS3134 , TMS570LS3134 , TMS570LS3135 , TMS570LS3135
Dbgauth facilitates debugger authentication on supported Texas Instruments SoC platforms. You will provide options that define the SoC being authenticated (-c, -m, -t), options that define the debugger environment (-x), and options that define inputs into the authentication algorithm (-k).
Based on the supplied SoC type, options are classified as required, optional, or N/A.
dbgauth is available as part of CCS EMUPACK releases. It can be found in:
CCS - <ccs_install>\ccs_base\common\uscif
Example:
dbgauth -c testBoard.dat -s ajsm -t cortexr4 -k 00112233445566778899AABBCCDDEEFF -m 1
Use the -h option for details on how to use the dbgauth tool.
The board.dat file needs to include the AJSM which has a 4-bit IR and is available at ICEPick port address 18.
Open the xml target configuration file from the download link in the abstract with CCS and click the test connection button. A test connection window will pop up and list the path to the generated board.dat file. The default path will be C:\users/<account name>\AppData\Local\TEXAS~1\CCS\ti\<#>\<#>\BrdDat\testboard.dat. Every time the button is pressed, this file will be overwritten; save a copy, if desired.