SNLU296A December   2022  – December 2022

 

  1.   DS560MB410EVM User's Guide
  2.   Trademarks
  3. 1Features
  4. 2Applications
  5. 3Ordering Information
  6. 4Setup
    1. 4.1 Modes of Programmable Communication
    2. 4.2 Configuration Overview
  7. 5SigCon Architect
    1. 5.1 Installation
    2. 5.2 Configuration
      1. 5.2.1 Establishing a Connection
      2. 5.2.2 Enabling Demo Mode
    3. 5.3 High Level Page
      1. 5.3.1 Device Status
      2. 5.3.2 Block Diagram
      3. 5.3.3 Crosspoint Switch
    4. 5.4 Low Level Page
    5. 5.5 EEPROM Page
    6. 5.6 Eye Height Page
  8. 6Common Problems and Suggested Solutions
  9. 7Bill of Materials
  10. 8EVM Cable Assemblies
  11. 9Revision History

Establishing a Connection

  1. Connect the computer to the DS560MB410 through a USB2ANY device and USB cable. If using a DS560MB410EVM, then this is accomplished by connecting the included USB cable to the EVM and computer. If using a stand alone USB2ANY device, then a connection can be made between the I2C pins on the USB2ANY and the SMBus pins on the DS560MB410. A common ground connection is also required.
  2. Ensure the DS560MB410 is in SMBus Target mode.
  3. Select appropriate SMBus address by using the Target Address menu.
  4. Select appropriate USB2ANY by using the USB2ANY Details menu.
  5. Click Apply to connect to the device. The status indicator at the bottom of SigCon Architect will turn green to indicate a successful connection.
GUID-20211209-SS0I-QFJN-5BHN-TWSK510DQH7J-low.pngFigure 5-5 Establishing a Connection with the DS560MB410