SNAA421 November 2025 LMK05318B , LMK5B12204 , LMK5B33216 , LMK5B33414 , LMK5C33216A , LMK5C33414A
The LMK device has a DPLL reference validation detector that checks the validity of the external DPLL reference input clock. The validity of the external DPLL reference is determined by the enabled detectors, outlined in Table 2-9. The status is reported by the "DPLL reference validation" bit, described in Table 2-13. Refer to Table 2-11 for the DPLL reference validation status registers in the LMK device families.
Note that the reference validation detectors do not apply to DPLL inputs that are sourced internally from a cascaded source. When using a cascaded source as the input, the reference validation bit is always 1 unless the upstream APLL is disabled or unlocked.
| DEVICE FAMILY | REFERENCE VALIDATION SETTING | DESCRIPTION |
|---|---|---|
| LMK05318B, LMK05318, LMK5B, LMK5CA, LMK5C | Validation timer | The setting is true when the DPLL reference remains valid (across all enabled detectors) for the time defined by the validation timer. |
| LMK05318B, LMK05318 | Amplitude detector | The setting is true when the voltage swing of the DPLL reference is higher than the defined amplitude threshold. |
| LMK05318B, LMK05318, LMK5B, LMK5CA, LMK5C | Frequency detector | The setting is true when the frequency error between DPLL reference and the XO input is within the valid threshold. If the frequency exceeds the invalid threshold, then the setting is false. Disable for 1PPS inputs. |
| LMK05318B, LMK05318, LMK5B, LMK5CA, LMK5C | Early (runt pulse) and late (missing pulse) window detectors | The setting is true when the period of the DPLL reference is less than the missing clock threshold and greater than the early clock threshold. Disable for 1PPS inputs. |
| LMK05318B, LMK05318, LMK5B, LMK5CA, LMK5C | Phase valid
monitor (1PPS phase detector) |
The setting is true when the next clock edge of the DPLL reference is within the expected clock edge defined by the detector threshold. Enable only for 1PPS inputs. |
| BIT STATE | MEANING | DESCRIPTION |
|---|---|---|
| 0 | Undesired result | The DPLL reference valid bit is cleared when the DPLL reference does not meet the requirements of the enabled reference validation settings. At least one of the enabled reference detectors is failing (false). |
| 1 | Desired result | The DPLL reference valid bit is set when the DPLL reference meets the requirements of the enabled reference validation settings. All of the enabled reference detectors must be passing (true). |
| DEVICE FAMILY | TICS PRO FIELD NAME | DPLL
REFERENCE VALID REGISTER |
|---|---|---|
| LMK05318B, LMK05318 | PRIREF_VALSTAT | R411[2] |
| SECREF_VALSTAT | R411[3] | |
| LMK5B, LMK5CA, LMK5C | REF0_VALID_STATUS | R50[0] |
| REF1_VALID_STATUS | R50[1] | |
| REF2_VALID_STATUS(1) | R50[2] | |
| REF3_VALID_STATUS(1) | R50[3] |