SLUUCG7 April 2024 BQ76922
| Class | Subclass | Name | Type | Min | Max | Default | Unit |
|---|---|---|---|---|---|---|---|
| Protections | COVL | Counter Dec Delay | U1 | 0 | 255 | 10 | s |
Description: Whenever a COV event occurs, the COV latch counter is incremented. While the counter is nonzero, it will be decremented after the delay set by this parameter. This parameter should be set to a value larger than Protections:Recovery:Time to ensure that repeated COV events can increment the counter faster than this would decrement it. This parameter should be set to a value smaller than Protections:COVL:Recovery Time to ensure that the latch counter is decremented before recovering. Otherwise, the protection would trigger again since the latch counter is still at the limit.