SLDA021B March 2014 – February 2020 AM3892 , AM3894
The solder paste manufacturer’s guidelines for reflow parameters should be applied when profiling PCBs. The components have soldered satisfactorily in tests with peak temperatures ranging from 230°C to 240°C, and TALs from 45 to 150 seconds.
The component’s body temperature should not exceed 260°C at any time during the reflow process.
The component’s body temperature should not exceed 255°C for more than 30 seconds.
An example of a typical soak profile is shown in Figure 4. It is a soak-style profile; straight ramp-style profiles such as the one seen in Figure 8 (rework section) are also acceptable.
Figure 4. Sample Reflow Profile