SLAA419C October 2009 – April 2019 MSP430F5418 , MSP430F5418A , MSP430F5419 , MSP430F5419A , MSP430F5435 , MSP430F5435A , MSP430F5436 , MSP430F5436A , MSP430F5437 , MSP430F5437A , MSP430F5438 , MSP430F5438A
One significant difference in the architecture of the F543xA MCUs is the replacement of the internal 1.5-V or 2.5-V reference (se the ADC12 block diagram in the MSP430F5xx and MSP430F6xx Family User's Guide) with a separate, general-purpose REF module that can provide voltages to the various analog peripherals on a given F5xx MCU. The implications to the application can be minimal, as the F543xA REF module includes a setting that is backward compatible with the F543x revisions of silicon (see Section 3 for details on enabling this mode). For the purpose of future compatibility, TI recommends using the REF module as a separate module and not in a backward-compatible mode.
At a high level, the improved features that the REF module provides are:
For details on how to use the REF module, see the MSP430F5xx and MSP430F6xx Family User's Guide.