Single Event Transients
SETs
are defined as heavy-ion-induced transients upsets on the DCLK of the ADC3683-SEP. SET
testing was performed at room temperature (no external temperature control applied).
DCLK SEUs were characterized using a positive edge trigger. The devices were
characterized with input voltages AVDD/IOVDD = 1.85V. To capture the event, the
NI-PXI-5172 Scope Card was continuously monitoring the DCLK. The DCLK was monitored by
using USER_LED3 that is located on the TSW1400EVM. The scope was attached to the LED
which would go high upon seeing that the FPGA was not receiving a valid clock signal.
The scope triggering from DCLK was programmed to record 20K samples with a sample rate
of 5M samples per second (S/s) in case of an event (trigger). Scope was programmed to
record 20% of the data before (pre) the trigger happened. Events were seen on DCLK and
are characterized below.
Table 7-2 lists the SET test conditions and results for all the data. The Results were analyzed
and broken down into
short and
long events based on time taken for the
DCLK to recover. A short event is defined by a transient which lasted less than 500ns
while a long event lasts greater than 500ns. An example of such events can be seen in
Figure 7-1 and
Figure 7-2.
Table 7-2 lists the SET test condition and results for all the data.
Table 7-1 Summary of ADC3683-SEP SET
Test Condition and Results
| Run Number |
Run Type |
Unit Number |
Temperature |
Ion |
Angle |
LETEFF (MeV × cm2/ mg) |
Flux (ions × cm2/ s) |
Fluence (ions × cm2) |
Count DCLK Events |
Count of Short Events |
Count of Long Events |
| 8 |
SEU |
1 |
Room |
109Ag |
0 |
51.12 |
1 × 102 |
1 × 105 |
1 |
1 |
0 |
| 9 |
SEU |
1 |
Room |
109Ag |
0 |
51.12 |
1 × 104 |
1 × 106 |
6 |
4 |
2 |
| 10 |
SEU |
1 |
Room |
63Cu |
0 |
21.44 |
1 × 102 |
1 × 105 |
3 |
1 |
2 |
| 11 |
SEU |
1 |
Room |
63Cu |
0 |
21.44 |
1 × 104 |
1 × 106 |
5 |
5 |
0 |
| 12 |
SEU |
1 |
Room |
63Cu |
0 |
21.44 |
1 × 105 |
1 × 107 |
50 |
43 |
7 |