ZHCSK61B August 2019 – December 2019 TPS66120 , TPS66121
PRODUCTION DATA.
The PPHV power path has an integrated temperature sensor to protect it from excessive heating. When the sensor in the path detects an overtemperature condition, the PPHV path will be automatically disabled (if enabled) and cannot be enabled until the overtemperature condition has been removed. FLT is asserted when an overtemperature event occurs.
In addition, the device has an integrated main temperature sensor. When the sensor detects an overtemperature condition, the PPHV power pathand the VBUS LDO of the device are completely disabled until the overtemperature condition has been removed.