SLVSHZ5 November 2026 TPS544628
ADVANCE INFORMATION
TOFF_FALL is shown in Figure 7-21 and described in Table 7-30.
Return to the Summary Table.
Write Transaction: N/A
Read Transaction: Read Word
Data Format: LINEAR11
NVM Back-up: EEPROM
Updates: On-the-fly The TOFF_FALL command sets the time, in milliseconds, from the end of the turn-off delay time until the reference DAC is commanded to 0mV. This command is used to cause the output voltage to decrease at a controlled rate, which effectively sets the slew rate of the reference DAC during the soft-off period. In the implementation of TOFF_FALL, the VREF DAC slew rate is adjusted for each of the supported 32 VBOOT levels to obtain a slew rate to have a soft-stop time close to (but not always exactly equal to) the target value. The selected slew rate for the 0.5ms TOFF_FALL is the same as shown in TON_RISE but with a negative slope. TOFF_FALL is scaled in the same manner as TON_RISE with the different settings. In practice, the VOUT fall time is not exactly equal to TOFF_FALL value since the device stops switching once the output voltage is discharged to 50mV.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| EXPONENT[4:0] | RESERVED | ||||||
| R-1Fh | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TOFF_FALL[3:0] | ||||||
| R-0h | R-Xh | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-11 | EXPONENT[4:0] | R | 1Fh | Linear format twos complement exponent. The exponent is not programmable, with a result of 0.5ms LSB. |
| 10-4 | RESERVED | R | 0h | Reserved |
| 3-0 | TOFF_FALL[3:0] | R | X | TOFF_FALL will be Read Only and will have the same values as programmed in TON_RISE. On reset the value will be determined by NVM. |