SLVSHZ5 November 2026 TPS544628
ADVANCE INFORMATION
The device requires input bypass capacitors between both pairs of VIN and PGND pins to bypass the power-stage. The bypass capacitors must be placed as close as possible to the pins of the IC as the layout allows. At least 20µF nominal of ceramic capacitance and two high-frequency ceramic bypass capacitors are required. A 0.1μF to 1μF capacitor must be placed as close as possible to both VIN pins 4 and 12 on the same side of the board of the device to provide the required high frequency bypass, to reduce the high frequency overshoot and undershoot on across the power-stage on the VIN and SW pins. TI recommends at least 1μF of bypass capacitance as close as possible to each VIN pin to minimize the input voltage ripple. The ceramic capacitors must be a high-quality dielectric of X6S or better for the high capacitance-to-volume ratio and stable characteristics across temperature. In addition to this requirement, more bulk capacitance can be needed on the input depending on the application to minimize variations on the input voltage during transient conditions.
Use Equation 22 to calculate the input capacitance required to meet a specific input ripple target. A recommended target input voltage ripple is 5% the minimum input voltage, 400mV in this example. The calculated input capacitance is 4.5μF. This example meets these two requirements with 2 × 10µF ceramic capacitors.
The capacitor must also have an RMS current rating greater than the maximum input RMS current in the application. Use Equation 24 to calculate the input RMS current the input capacitors must support. The result is 3A in this example. The ceramic input capacitors have a current rating greater than this value.
For applications requiring bulk capacitance on the input, such as ones with low input voltage and high current, TI recommends the selection process in How to select input capacitors for a buck converter analog design journal.