SLVSHK4 December 2025 MCT8376Z-Q1
PRODUCTION DATA
The Hall sensor inputs on the MCT8376Z-Q1 device can interface with a variety of Hall sensors. Typically, a Hall element is used, which outputs a differential signal. To use this type of sensor, the AVDD regulator can be used to power the Hall sensor. Figure 9-3 shows the connections.
Figure 9-3 Typical Hall Sensor ConfigurationBecause the amplitude of the Hall-sensor output signal is very low, capacitors are often placed across the Hall inputs to help reject noise coupled from the motor. Capacitors with a value of 1 nF to 100 nF are typically used.