ZHCSFO3D November 2016 – August 2021 LM5170-Q1
PRODUCTION DATA
The LM5170-Q1 monitors the real time inductor current in each channel at the IOUT1 and IOUT2 pins. The channel current is converted to a small current source scaled by the factors seen in Equation 11 and Equation 12:


where
The DC offset current is introduced to raise the no-load signal above the possible ground noise floor. Because the monitor signal is in the form of current, an accurate reading can be obtained across a termination resistor even if the resistor is located far from the LM5170-Q1 but close to the MCU, thus rejecting potential ground differences between the LM5170-Q1 and the MCU. Figure 8-6 shows a typical channel current monitor through a 9.09-KΩ termination resistor and a 10-nF to 100-nF ceramic capacitor in parallel. The RC network converts the current monitor signal into a DC voltage proportional to the channel DC current. For example, when the current sense voltage DC component is 50 mVdc, namely VCS_dc = 50 mV, the termination RC network will produce a DC voltage of 2.5 V. Note that the maximum IOUT pin voltage is internally clamped to approximately 4 V.
Figure 8-5 Channel Monitor Current Source vs Current Sense Voltage
Figure 8-6 Channel Current Monitor