ZHCSLR1B December 2021 – December 2021 LDC3114-Q1
PRODUCTION DATA
The COM pin requires a bypass capacitor to ground. The capacitor should be a low-ESL, low-ESR type. CCOM must be sized so that the following relationship is valid for all channels.
The value of QSENSORn when the sensor is at the minimum target distance should be used. The maximum acceptable value for CCOM is 20 nF. The CCOM range for a particular sensor configuration can be obtained with the Spiral_Inductor_Designer tab of the LDC Calculations Tool.