ZHCSQT2 March 2024 ADS127L18
ADVANCE INFORMATION
Power-supply rejection ratio (PSRR) specifies the ability of the ADC to reject power-supply interference. PSRR is expressed as ac and dc parameters. For PSRR (dc) measurement, the power-supply voltage is changed over the minimum, nominal, and maximum specified voltage ranges with the inputs externally shorted together. The maximum change of ADC offset voltage is recorded versus the change in power-supply voltage. PSRR (dc) is computed as shown in Equation 12 as the ratio of change of the power-supply voltage step to the change of offset voltage.
where:
For the measurement of PSRR (ac), the power-supply voltage is modulated by a 100mVpp (35mVRMS) signal at various test frequencies. An FFT of the ADC data with power-supply modulation is performed. Equation 7 shows that the nine largest amplitude spurious frequencies in the frequency spectrum are summed as powers. These frequencies are then related to the amplitude of the power-supply modulation signal.
where: