TIDUEY0A November 2020 – December 2025
Use the following steps to run the code for Lab 5:
from the menu bar.BT4CH_InputVoltageSense_V is from 12V to 15V in the Expression Window.BT4CH_userParam_chX->Relay_ON to 1 to enable the
output relayBT4CH_userParam_chX->iref_A = 5.0BT4CH_userParam_chX->vrefCharge_V = 3BT4CH_userParam_chX->en_bool = 1BT4CH_measureVI_chX variable shows output current and voltage of the DC/DC converter.BT4CH_userParam_chX->Dir_bool.BT4CH_userParam_chX->iref_A = 0BT4CH_userParam_chX->vrefCharge_V = 0BT4CH_userParam_chX->en_bool = 0BT4CH_userParam_chX->Relay_ON to 0 to disable
the output relay
Figure 3-32 Lab 5 Expression
Windows