SWRU640 March 2026
The previous section discussed how to connect two devices in a stack configuration, enabling communication from COMH to COML, known as the "north direction." Alternatively, users can opt for a "Ring Architecture" setup. In this configuration, a daisy chain cable connects COMH of the base to COML of the bottommost stack (S1), while also linking COML of the base to COMH of the topmost stack.
This arrangement facilitates communication in both the north and south directions, ensuring communication from COML to COMH as well. Consequently, even if there's a break in the daisy chain, the base device maintains communication with all devices in the stack.