SWRU640 March 2026
U9 is the TPS3436-Q1 watchdog timer used to monitor the CC2662R-Q1 device. If the CC2662R-Q1 hangs because of a SW error or HW issue, the watchdog timer will drive the CC2662R-Q1 reset line low to reset the device.
Figure 2-18 U9 TPS3436-Q1 Watchdog Timer