10.2.2 Station
The following tables list all of the parameters applicable for Station group.
| Parameter |
Mac Address |
| Description |
device MAC address |
| Options |
6 bytes valid MAC address written in HEX format and separated by ‘:’ or ‘-‘, (12:34:56:78:90:ab). Note that it is restricted to set the LSB of the most significant byte |
| Dependencies |
None |
| Parameter |
Station Tx Power Level |
| Description |
Back-off number from maximum power. Applicable for Station and Peer2Peer client roles only |
| Options |
Number in range 0-15, dB units |
| Dependencies |
None |
| Parameter |
Power Policy |
| Description |
Power policy of the device |
| Options |
Single selection between PM_NORMAL, PM_ACTIVE and PM_LONG_SLEEP |
| Dependencies |
None |
| Parameter |
Long Sleep Interval |
| Description |
Denotes the desired sleep interval between two consecutive wakeups for beacon reception |
| Options |
Interval in mSec units |
| Dependencies |
Applies only when Power Policy is set to PM_LONG_SLEEP |
| Parameter |
Scan Channel Mask |
| Description |
Channels mask during scan process |
| Options |
Multiple choice between Channel1-Channel13 |
| Dependencies |
None |
| Parameter |
Scan RSSI Threshold |
| Description |
RSSI threshold during scan process |
| Options |
Negative number in dBm units, represented as 2's complement |
| Dependencies |
None |
| Parameter |
Station Addressing Scheme |
| Description |
Setting static IP parameters or get it dynamically via DHCP |
| Options |
Static or Dynamic. Applicable to station and Peer2Peer client roles only |
| Dependencies |
None |
| Parameter |
Station IP Address |
| Description |
IP address |
| Options |
Valid IP address separated by ‘.’, (192.168.1.1). Applicable to station and Peer2Peer client roles only. Note that Station IP and Station Default Gateway must reside on the same network. |
| Dependencies |
Applies only when Station Addressing Scheme is set to Static |
| Parameter |
Station Subnet Mask |
| Description |
Subnet mask |
| Options |
Valid subnet mask separated by ‘.’, (255.255.255.0). Applicable to station and Peer2Peer client roles only |
| Dependencies |
Applies only when Station Addressing Scheme is set to Static |
| Parameter |
Station Default Gateway |
| Description |
Default gateway |
| Options |
Valid IP address separated by ‘.’, (192.168.1.254). Applicable to station and Peer2Peer client roles only. Note that Station IP and Station Default Gateway must reside on the same network. |
| Dependencies |
Applies only when Station Addressing Scheme is set to Static |
| Parameter |
Station DNS Server |
| Description |
DNS Server |
| Options |
Valid IP address separated by ‘.’, (192.168.1.254). Applicable to station and Peer2Peer client roles only |
| Dependencies |
Applies only when Station Addressing Scheme is set to Static |
| Parameter |
Station Network Applications |
| Description |
Enabled network applications |
| Options |
Multiple choices between HTTP server, mDNS client and Device configuration. Applicable to station role only |
| Dependencies |
None |