SWRU558 June 2020 CC3100 , CC3100MOD , CC3200 , CC3200MOD
There are two ways to load a session:
Choosing an existing .usf file, UniFlash will be populated with the same template, token and other GUI changes from the saved session. Once loaded, any changes that users perform in the GUI will automatically be saved to the same configuration.
Figure 4. Loading a Session
Figure 5. Loading a Session From a Bar