SWRU558 June   2020 CC3100 , CC3100MOD , CC3200 , CC3200MOD

 

  1.   SimpleLink Wi-Fi CC3100, CC3200 UniFlash
    1.     Trademarks
    2. Introduction
      1. 1.1 Overview
    3. Installation
      1. 2.1 Linux
        1. 2.1.1 Limitations
        2. 2.1.2 During Installation
        3. 2.1.3 Running UniFlash
        4. 2.1.4 C++ Dependencies
        5. 2.1.5 COM Port
        6. 2.1.6 Porting Between Windows and Linux
    4. Prerequisites
      1. 3.1 Software
      2. 3.2 Hardware
    5. Uniflash Block Diagram
    6. Session Support
      1. 5.1 Overview
      2. 5.2 Session Conversion
      3. 5.3 Creating a Session
        1. 5.3.1 Session Content
        2. 5.3.2 Creation Procedure
        3. 5.3.3 Relative Path Support
      4. 5.4 Saving a Session
      5. 5.5 Loading a Session
    7. Secured File System Support
    8. GUI Interface
      1. 7.1 Main Screen
      2. 7.2 Target Connection
      3. 7.3 Format
      4. 7.4 Get Version
      5. 7.5 File Programming
        1. 7.5.1 General
        2. 7.5.2 Non-Secured File Programming
        3. 7.5.3 Secured File Programming
      6. 7.6 Service Pack Programing
        1. 7.6.1 General
        2. 7.6.2 Procedure
      7. 7.7 Adding a New File to the Device
      8. 7.8 Erasing Existing File From the Device
      9. 7.9 Removing Existing File From the Template
    9. CC3200 Support
      1. 8.1 Overview
      2. 8.2 Configuration and Programing
    10. Command Line Support
      1. 9.1 Overview
      2. 9.2 Programming
        1. 9.2.1 Command Line Syntax
        2. 9.2.2 Help Manual
      3. 9.3 Available Options
        1. 9.3.1 Available Operations
        2. 9.3.2 Legend
        3. 9.3.3 Programming Example
    11. 10 Configuration File Support
      1. 10.1 Overview
      2. 10.2 Configuration Groups – Parameters’ Description
        1. 10.2.1 Device Role
        2. 10.2.2 Station
        3. 10.2.3 Access Point (AP)
        4. 10.2.4 Peer 2 Peer (P2P)
        5. 10.2.5 Profiles
        6. 10.2.6 HTTP Server
        7. 10.2.7 DHCP Server
        8. 10.2.8 mDNS Client
        9. 10.2.9 Smart Config
      3. 10.3 Configuration Groups – GUI Interface
        1. 10.3.1 Device Role
          1. 10.3.1.1 Restore to Default
          2. 10.3.1.2 Programming
          3. 10.3.1.3 Generation of Binary Templates
          4. 10.3.1.4 Configuration
        2. 10.3.2 Station
          1. 10.3.2.1 Restore to Default
          2. 10.3.2.2 Programming
          3. 10.3.2.3 Generation of Binary Templates
          4. 10.3.2.4 Flow
          5. 10.3.2.5 Configuration
        3. 10.3.3 Access Point (AP)
          1. 10.3.3.1 Restore to Default
          2. 10.3.3.2 Programming
          3. 10.3.3.3 Generation of Binary Templates
          4. 10.3.3.4 Flow
          5. 10.3.3.5 Configuration
        4. 10.3.4 Peer 2 Peer (P2P)
          1. 10.3.4.1 Restore to Default
          2. 10.3.4.2 Programming
          3. 10.3.4.3 Generation of Binary Templates
          4. 10.3.4.4 Flow
          5. 10.3.4.5 Configuration
        5. 10.3.5 HTTP Server
          1. 10.3.5.1 Restore to Default
          2. 10.3.5.2 Programming
          3. 10.3.5.3 Generation of Binary Templates
          4. 10.3.5.4 Flow
          5. 10.3.5.5 Configuration
        6. 10.3.6 DHCP Server
          1. 10.3.6.1 Restore to Default
          2. 10.3.6.2 Programming
          3. 10.3.6.3 Generation of Binary Templates
          4. 10.3.6.4 Flow
          5. 10.3.6.5 Configuration
        7. 10.3.7 mDNS Client
          1. 10.3.7.1 Restore to Default
          2. 10.3.7.2 Programming
          3. 10.3.7.3 Generation of Binary Templates
          4. 10.3.7.4 Adding/Deleting a Service
          5. 10.3.7.5 Flow
          6. 10.3.7.6 Configuration
        8. 10.3.8 Profiles
          1. 10.3.8.1 Restore to Default
          2. 10.3.8.2 Programming
          3. 10.3.8.3 Generation of Binary Templates
          4. 10.3.8.4 Adding/Deleting a Profile
          5. 10.3.8.5 Flow
          6. 10.3.8.6 Configuration
        9. 10.3.9 Smart Config
          1. 10.3.9.1 Restore to Default
          2. 10.3.9.2 Programming
          3. 10.3.9.3 Generation of Binary Templates
          4. 10.3.9.4 Flow
          5. 10.3.9.5 Configuration
    12. 11 Image Creation and Programming
      1. 11.1 Overview
      2. 11.2 Basic Concept and Operation
      3. 11.3 Image Creation – Supported Commands
        1. 11.3.1 Overview
        2. 11.3.2 General Settings
        3. 11.3.3 Format Storage Command
        4. 11.3.4 Write Service Pack Command
        5. 11.3.5 Write File Command
        6. 11.3.6 Write Gang Image Command
        7. 11.3.7 Start Logger Command
      4. 11.4 Image Creation – GUI Interface
        1. 11.4.1 Image Programming Summary Window
        2. 11.4.2 Image Programming Buttons
          1. 11.4.2.1 Add
          2. 11.4.2.2 Remove
          3. 11.4.2.3 Move
          4. 11.4.2.4 Program
          5. 11.4.2.5 Export
          6. 11.4.2.6 Settings
      5. 11.5 Image Programming to Target
      6. 11.6 How to Build an Image Guide
      7. 11.7 Serial Flash usage and Design
        1. 11.7.1 Overview
        2. 11.7.2 File System Guidelines
        3. 11.7.3 Memory Usage
          1. 11.7.3.1 Device Generic
          2. 11.7.3.2 Image Specific
      8. 11.8 Image Creation – Troubleshooting
    13. 12 Troubleshoot/Debugging
    14. 13 Limitations
    15. 14 References
  2.   A UART Connection
    1.     A.1 UART Connection

Access Point (AP)

The following tables list all of the parameters applicable for AP group.

Parameter Mac Address
Description device MAC address
Options 6 bytes valid MAC address written in HEX format and separated by ‘:’ or ‘-‘, (12:34:56:78:90:ab). Note that it is restricted to set the LSB of the most significant byte
Dependencies None
Parameter SSID
Description SSID indicates the name of the network in AP role
Options SSID is a string up to 32 bytes
Dependencies None
Parameter Security Type
Description WiFi Security Type in AP role
Options Single selection between Open, WEP and WPA
Dependencies None
Parameter WEP Key Format
Description WEP key format in AP role
Options Either Hexadecimal or ASCII
Dependencies None
Parameter Password
Description WiFi password in AP role
Options For WEP, it is either 5 bytes or 13 bytes, Hexadecimal or ASCII format. For WPA, it is 8-63 bytes
Dependencies Applies only when Security Type is set to WEP or WPA
Parameter Country Code
Description Country Code for regulatory purposes
Options Single choice between US, EU and JP
Dependencies None
Parameter Channel
Description Operating WiFi channel
Options Single choice between Channel x, where x denotes the channel number 1-13
Dependencies None
Parameter Hidden SSID
Description Setting this option makes SSID not being broadcast in AP role
Options Boolean, False or True
Dependencies None
Parameter Device Domain Name
Description In AP role, part of the default SSID
Options String up to 33 bytes
Dependencies None
Parameter AP Tx Power Level
Description Back-off number from maximum power. Applicable for AP and Peer2Peer group owner roles only
Options Number in range 0-15, dB units
Dependencies None
Parameter Ignore Force AP
Description Applicable for CC3100 only. In case AP is forced via GPIO, setting this option makes the device boot as open AP
Options Boolean, False or True
Dependencies None
Parameter Beacon Interval
Description Beacon Interval is the interval between AP beacons notifications
Options It is represented in TUs where each TU (Time Unit) is 1024 µSec
Dependencies None
Parameter DTIM Interval
Description DTIM Interval is the interval between beacons containing broadcast information
Options It is represented in Beacon Intervals
Dependencies None
Parameter AP Addressing Scheme
Description Setting static IP parameters or get it dynamically via DHCP
Options Static or Dynamic. Applicable to AP and Peer2Peer group owner roles only
Dependencies None
Parameter AP IP Address
Description IP address
Options Valid IP address separated by ‘.’, (192.168.1.1). Applicable to AP and Peer2Peer group owner roles only. Note that AP IP and AP Default Gateway must reside on the same network.
Dependencies None
Parameter AP Subnet Mask
Description Subnet mask
Options Valid subnet mask separated by ‘.’, (255.255.255.0). Applicable to AP and Peer2Peer group owner roles only
Dependencies None
Parameter AP Default Gateway
Description Default gateway
Options Valid IP address separated by ‘.’, (192.168.1.254). Applicable to AP and Peer2Peer group owner roles only. Note that AP IP and AP Default Gateway must reside on the same network.
Dependencies Applies only when AP Addressing Scheme is set to Static
Parameter AP DNS Server
Description DNS Server
Options Valid IP address separated by ‘.’, (192.168.1.254). Applicable to AP and Peer2Peer group owner roles only
Dependencies Applies only when AP Addressing Scheme is set to Static
Parameter AP Network Applications
Description Enabled network applications
Options Multiple choices between HTTP server, mDNS client, DNS Server and Device configuration. Applicable to AP role only
Dependencies None