SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
The following configuration is required to measure the frequency of an event source waveform. Use the sequence that follows:
Figure 20-17 shows a generic event source waveform.
Figure 20-17 Frequency Measurement Waveform
The TDC measures correct signal frequency if the selected event source waveform matches the requirements listed in Table 20-25.
| Description | Label | Requirement |
|---|---|---|
| Minimum low time | t_minL | 208 ns |
| Minimum high time | t_minH | 208 ns |
| Minimum period | t_min | 416 ns |
If an event waveform does not directly fulfill these requirements, the user must complete the following sequence:
Fore more details, see Section 20.4.5.2.6.