SPRZ292S December   2008  – November 2020 TMS320F28020 , TMS320F280200 , TMS320F28021 , TMS320F28022 , TMS320F28022-Q1 , TMS320F280220 , TMS320F28023 , TMS320F28023-Q1 , TMS320F280230 , TMS320F28026 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027 , TMS320F28027-Q1 , TMS320F280270 , TMS320F28027F , TMS320F28027F-Q1

 

  1.   TMS320F2802x, TMS320F2802xx MCUs Silicon Revisions B, A, 0
  2. 1Introduction
  3. 2Device and Development Support Tool Nomenclature
  4. 3Device Markings
  5. 4Usage Notes and Known Design Exceptions to Functional Specifications
    1. 4.1 Usage Notes
      1. 4.1.1 PIE: Spurious Nested Interrupt After Back-to-Back PIEACK Write and Manual CPU Interrupt Mask Clear Usage Note
      2. 4.1.2 Flash: MAX "Program Time” and “Erase Time” in Revision O of the TMS320F2802x Microcontrollers Data Manual are only Applicable for Devices Manufactured After October 2020
    2. 4.2 Known Design Exceptions to Functional Specifications
      1.      Advisory to Silicon Variant / Revision Map
      2.      Advisory
      3.      Advisory
      4.      Advisory
      5.      Advisory
      6.      Advisory
      7.      Advisory
      8.      Advisory
      9.      Advisory
      10.      Advisory
      11.      Advisory
      12.      Advisory
      13.      Advisory
      14.      Advisory
      15.      Advisory
      16.      Advisory
      17.      Advisory
      18.      Advisory
      19.      Advisory
      20.      Advisory
      21.      Advisory
      22.      Advisory
  6. 5Documentation Support
  7. 6Trademarks
  8. 7Revision History

Advisory to Silicon Variant / Revision Map

Table 4-2 List of Advisories
TITLE SILICON REVISION(S) AFFECTED
0 A(1) B(1)
ADC: Temperature Sensor Minimum Sample Window Requirement Yes Yes Yes
ADC: DC Specifications: Linearity Limitation Yes Yes Yes
ADC: Offset Self-Recalibration Requirement Yes Yes Yes
ADC: Out-of-Specification Current Consumption on Power Up Yes Yes Yes
ADC: ADC Result Conversion When Sampling Ends on 14th Cycle of Previous Conversion, ACQPS = 6 or 7 Yes Yes Yes
ADC: Initial Conversion Yes Yes Yes
ADC: ADC can Become Non-Responsive When ADCNONOVERLAP or RESET is Written During a Conversion Yes Yes Yes
ADC: New ADC Control Bits Added to Revision A Silicon Yes Yes
BOR: BOR Trip Point Limits VDDIO Tolerance Yes Yes Yes
Memory: Prefetching Beyond Valid Memory Yes Yes Yes
GPIO: GPIO Qualification Yes Yes Yes
Watchdog: Incorrect Operation of CPU Watchdog When WDCLK Source is OSCCLKSRC2 Yes Yes Yes
Oscillator: CPU Clock Switching to INTOSC2 May Result in Missing Clock Condition After Reset Yes Yes Yes
Flash: Flash API v2.00 Software Library Cannot be Used on the TMS320F28020 and TMS320F280200 Devices Yes Yes Yes
ePWM: An ePWM Glitch can Occur if a Trip Remains Active at the End of the Blanking Window Yes Yes Yes
ePWM: Trip Events Will Not be Filtered by the Blanking Window for the First 3 Cycles After the Start of a Blanking Window Yes Yes Yes
Boot ROM: Flash API [Flash_Erase( ) Function] Yes Yes Yes
Boot ROM: Flash API [Flash_Program( ) Function] Yes
Zero-Pin Oscillator: Modification to Oscillator Frequency Parameter Yes Yes
CPU: PCLKCR0[14] Setting May Stall CPU Yes
VREG: VREG Minimum VDD Output Voltage for TMP Devices is Below Data Sheet Limit Yes
The difference between revision A silicon and revision B silicon is the addition of the InstaSPIN™ code in revision B silicon. The InstaSPIN code in secure ROM is execute-only with no read access. For more details, see the TMS320F28026F, TMS320F28027F InstaSPIN™-FOC Software Technical Reference Manual. In revision B silicon, the original ROM contents from revision A silicon have not been modified. All new additions for revision B silicon have been placed in the unused locations of ROM in revision A silicon. However, the ROM revision code has been updated on revision B and the ROM checksum will be different between the two revisions.