SPRACQ1 May 2020 TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377S , TMS320F28379D , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Similar to F2837x, F2838x supports the XCLKOUT feature. On F2838x, the following additional source has been added to XCLKOUT. Because of this, the LKSRCCTL3.XCLKOUTSEL register bit field has been extended to 4 bit instead of 3.
| XCLKOUTSEL | F2838x | F2837x |
|---|---|---|
| 000 | PLLSYSCLK (default on reset) | PLLSYSCLK (default on reset) |
| 001 | SYSPLLCLK | PLLRAWCLK |
| 010 | CPU1.SYSCLK | CPU1.SYSCLK |
| 011 | CPU2.SYSCLK | CPU2.SYSCLK |
| 100 | AUXPLLCLK | AUXPLLRAWCLK |
| 101 | INTOSC1 | INTOSC1 |
| 110 | INTOSC2 | INTOSC2 |
| 111 | XTAL OSC (o/p clock) | Reserved |
| 1000 | CMCLK | NA |
| 1100 | PLLRAWCLK | NA |
| 1101 | AUXPLLRAWCLK | NA |
| others | Reserved | NA |
Also on the F2838x devices, XCLKOUT has been connected to one of the inputs of the OUTPUTXBAR switch to provide more flexibility to user.