SPNU634 January 2020 RM42L432 , RM44L520 , RM44L920 , RM46L430 , RM46L440 , RM46L450 , RM46L830 , RM46L840 , RM46L850 , RM46L852 , RM48L530 , RM48L540 , RM48L730 , RM48L740 , RM48L940 , RM48L950 , RM48L952 , RM57L843 , TMS570LC4357 , TMS570LC4357-EP , TMS570LC4357-SEP , TMS570LS0332 , TMS570LS0432 , TMS570LS0714 , TMS570LS0714-S , TMS570LS0914 , TMS570LS1114 , TMS570LS1115 , TMS570LS1224 , TMS570LS1225 , TMS570LS1227 , TMS570LS2124 , TMS570LS2125 , TMS570LS2134 , TMS570LS2135 , TMS570LS3134 , TMS570LS3135 , TMS570LS3137 , TMS570LS3137-EP
Choose Texas Instruments Code Composer v5.0 (Default) (see Figure 2).
Figure 2. Compiler Selection Leave it as default (see Figure 3).
Figure 3. Coverage Selection Leave it as default or browse to the desired editor.
Figure 4. Source Code Browser Selection Default: c:\ti\ccs5\ (see Figure 5).
Browse to the latest TI CCS installation folder CCS5 or CCS6.
Figure 5. Choose TI CCS Install Path Leave it as default to LDRA.
Figure 6. Project Configuration er or not the LDRA FlexLM license server is up and running by doing the following steps.
NOTE
The License Configuration Manager must be run as Admin.
Figure 7. Run License Configuration Manager as Admin
Figure 8. LDRA License Configuration NOTE
IF you see the FlexLM Server Status as
, either the License is expired or the FlexLM service is not started. Restart or start the FlexLM License Service in the Windows as shown in Figure 9.
Figure 9. Start or Restart FlexLM Server Status