SLUUCC4A October   2020  – September 2021 TPS92520-Q1

 

  1.   Trademarks
  2.   General Texas Instruments High Voltage Evaluation (TI HV EMV) User Safety Guidelines
  3. 1Description
    1. 1.1 Typical Applications
    2. 1.2 Warnings
    3. 1.3 Connector Description
  4. 2Performance Specifications
  5. 3Performance Data and Typical Characteristic Curves
    1. 3.1 1.5A CC BUCK SW-Node Voltage Waveform
    2. 3.2 Start-up Waveforms
    3. 3.3 PWM Dimming
  6. 4Schematic, PCB Layout, and Bill of Materials
    1. 4.1 Schematic
    2. 4.2 Layout
    3. 4.3 Bill of Materials
  7. 5Software
    1. 5.1 Demonstration Kit Software Installation for LEDMCUEVM-132 Board
      1. 5.1.1 Installation Overview
    2. 5.2 Step-by-Step Installation Instructions
    3. 5.3 Installation Error Recovery
    4. 5.4 Checking for Updates
  8. 6TPS92520EVM-133 Power Up and Operation
    1. 6.1 Power Up and Operation at VINx < 40 V
    2. 6.2 MCU Control Window
    3. 6.3 SPI Command Window
    4. 6.4 Watchdog Window
    5. 6.5 GUI Devices Window
      1. 6.5.1 Channel 1 or 2 Sub-Window: Settings, Measurements, and Faults
      2. 6.5.2 Device Sub-Window: Shared Device Settings, Measurements, Register Info, and Limp Home
    6. 6.6 Limp Home Mode Window
  9. 7Revision History

GUI Devices Window

The device command window will not do any reads of the device until the En 520 No WD button has been selected and the watch dog timer has been disabled, see Figure 6-18 .

GUID-20200811-CA0I-J0BP-NN3T-4TXFK2QV04KV-low.gifFigure 6-18 Device Command Window

Once the En 520 No WD has been selected, the GUI will perform an initial read of all the registers and load the information into the device command window, shown in Figure 6-19. Note that SHORT, BSTUV, and STATUS are flagged red because those faults conditions have occurred. The SHORT fault condition occurs because the output is off and no current is driving the LEDs and the voltage at the output is less than 2.45 V on the CSP pin, which indicates a SHORT condition. BSTUV fault indicates that the bootstrap supply is lower than 2.95 V, which is correct because the booststrap voltage is created when the output is turned on and the switch node is pulled to ground to charge the booststrap capacitor to drive the high-side FET. STATUS fault indicates that a fault has occurred and is the logic OR of the fault bits for that channel.

The GUI is split up into different sub windows for each the Devices. There can be multiple tabs (Devices) and each tab will be for a specific device at at specific SPI address. Figure 6-19 shows the TPS92520 (520) as the device and the address (Addr) is 0.

GUID-20200824-CA0I-XQJZ-SNFQ-KK84BFH3DM2L-low.gif Figure 6-19 Devices Window After Watchdog is Disabled.
There are sub-windows for each channel ( Channel 1 and Channel 2) and the Device sub-window for shared features. The Device window covers features for the device such as thermal, faults, fault timer settings, PWM frequency, limp home mode, 5VD measurements, fault resets, sleep mode, and register reads. Each channel window sets the LED current (Analog Current), switching frequency (On Time), the PWM duty cycle (PWM), PWM source (Internal or External UDIM pin), fault response settings, and if the channel is enabled or not. The channel windows also have information about input voltage (VIN) and output LED voltage (LED) measurements. There are also the associated status information such as fault flags that are tied to each channel.